MODBUS.KEEPALIVE

Description

Enables or disables the Modbus keepalive fault.

AKD2G uses TCP keepalive to monitor the Ethernet connection between the AKD2G and the HMI. If the connection is unexpectedly terminated, for example the cable is cut, the Modbus keepalive fault F7101 is generated.

0 = Disabled. The Modbus keepalive fault will not be generated.
1 = Enabled (default). The Modbus keepalive fault is generated and a fault occurs for both axes.

Example

The following stops the Modbus keepalive from being processed.

-->MODBUS.KEEPALIVE 0
-->

Context

For more information, see Handling Broken Connections.

Versions

Action Version Notes

Implemented

02-05-00-000

 

General Information

Type

Read Write Parameter

Units

N/A

Range

0 or 1

Default Value

1

Data Type

Integer

See Also

Fault F7101

Stored in Non-Volatile Memory

Yes

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

MODBUS.KEEPALIVE

3014h

04h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

MODBUS.KEEPALIVE

3706

E7A

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

MODBUS.KEEPALIVE

3706

Unsigned8

Read/Write

-